machine vision and identification
Application
REST API of the sensingCam SEC100
Functionality, authentication and settings of the REST API with example.
Field of View Calculation of the sensingCam SEC100
Supplementary calculation of the Field of View (FoV) based on the horizontal and vertical detection angle.
Tips for the stream settings and network load reduction of the sensingCam SEC100
For some applications it might be necessary to reduce the network load when using the sensingCam SEC100. This article is about tips for reducing this load.