motion control sensors
Application
(Show all)What points need to be checked if programming with the PGT-08-S/1036616 does not work?
What points need to be checked if programming with the PGT-08-S/1036616 does not work?
What measuring wheel circumferences are possible to mount on the spring arm mechanic of the DBV50?
FAQ
(Show all)Has the hardware design of the PGT-08-S/1036616 changed? What points need to be considered before operating the PGT-08-S?
Has the hardware design of the PGT-08-S/1036616 changed? What points need to be considered before operating the PGT-08-S?
Are there older SDD files than V2.3 for the PGT-08-S available to program incremental and absolute encoders?
Is there an overview for the needed tool to tighten the clamping ring screw from all hollow shaft encoders?