LiDAR and radar sensors
Application
Description
This article provides additional information and instructions to the CoLa A and CoLa B protocol as well as the corresponding software modules and examples.
Entry point for LiDAR ROS Driver
Description
Describes how to measure different types of meteorology in fog conditions.
Description
Description
Description
Description
Description
Every single measurement degree (TiM has a resolution of 0.33° or 1°) consists of 84 single measurement points that are accumulated for one measurement value output.