Safety
Application
(Show all)What points need to be checked if programming with the PGT-08-S/1036616 does not work?
What points need to be checked if programming with the PGT-08-S/1036616 does not work?
FAQ
(Show all)Has the hardware design of the PGT-08-S/1036616 changed? What points need to be considered before operating the PGT-08-S?
Has the hardware design of the PGT-08-S/1036616 changed? What points need to be considered before operating the PGT-08-S?
Are there older SDD files than V2.3 for the PGT-08-S available to program incremental and absolute encoders?
Is is possible to mount a face mount flange encoder with a centering of 36mm on the spring arm from the measuring wheel encoder DBV50?
Tutorial
(Show all)The STL70 (Hiperface) in combination with the PGT-11