detection sensors
Application
This article provides an example of printed circuit board detection using through beam optical fibers and amplifiers.
The article explains how to detect a certain side of a beam splitter.
This article shows how to configure an fiber amplifier to detect ultra small holes in a circuit board using SopasET.
using the example of the WLL80 light guide sensor, the difference between visible red light and invisible longer-wave IR is shown
This article shows a simple method of detecting ultra small dark SMD parts on a bright surface by using fiber optics.
Reasons and how to prevent drifting of received light value when using fibers
This article shows how to detect a small object at a distance of 800mm with throughbeam fibers.
"locating lug" or embossing detection on turning bottle with fiber
The article answers the question as to how one can reach the minimum detectable object with a fiber amplifier.
The article suggests a solution on how to detect the turning position of a bottle with a flat part for labeling.
The article informs about shock, vibration, temperature and humidity resistance of SICK sensors.
Check if Cap is in Correct Position with Proximity Fiber
Application example: How to detect 5 threads in a metal housing with WLL180 (or WLL80).
The article suggests fiber amplifier eg. WLL180T or WLL80 and fiber optic LL3-TF01 to detect bubbles in liquid.
The article describes how to detect objects below the water surface using fiber optics with teflon sleeve.
Paper jam detection on flatbed printer with fiber optic, fiber with ir-block-filter #5328271, LL3-TA01IR
Application example on how to detect a clear window in an envelope body using fiber optic and proximity fiber.
The article describes how to detect package edges with a fiber optic amplifier WLL80 or WLL190T.