detection sensors
Application
Optical synchronization simplifies installation and reduces wiring complexity. Maintaining one clear SYNC beam is critical for full functionality.
Description
The article explains how to use the MLG-2 to measure the center point of a box.
The article informs about shock, vibration, temperature and humidity resistance of SICK sensors.
This article describes how to measure the height position of a very thin metal sheet with MLG-2 Pro and LBH.
The article explains how to use the MLG2 Pro to differentiate between various types of pallets via "object recognition".
Measuring accuracy of the MLG-2 WebChecker
This article informs about MLG-2 height measurement using BBH (Blocked Beams Hold).
The article describes how to detect holes in transparent films by using MLG-2.
This article explains how to mount the angle holder.
The article illustrates how to count all kinds of bottles with different sizes by using a MLG-2 Pro.
The article answers the question whether or not the WebChecker MLG is suited for thicker objects and lists some restrictions - Part 1.
This article shows how to monitor luggage on a conveyor belt with the MLG-2 Pro used for tracking the profile.
The article suggests different solutions for ejection control (FLG vs MLG2-Pro).
The article provides information about the MLG2 Pro alignment help in SOPAS.
Explains how to increase the resolution of a light curtain using the MLG-2.
The article informs about the response time, minimum presence time & reproducibility of a MLG-2 and MLG-2 ProNet.
This article compares old versus new M12-8-Pin cables.
This article explains how to map diagnosis to left Q outputs in order to get diagnosis information on the MLG-2 Pro.
This article explains how to check if the MLG-2 is fast enough / how to calculate the maximum speed possible.
The article shows how to measure thick objects with a MLG-2.