distance sensors
Application
(Show all)Setting up a serial communication (RS232 or RS422) to the OD7000
Description
What is refractive index and why it is important
Explanation of refractive index and importance for thickness measurement of transparent materials
Measuring into holes with the OD7000
Description
FAQ
(Show all)In which wavelength range does the OD7000 light source emit?
Description
Why does OD7000 not give me the actual distance to the target surface ?
Explanation of working distance, measuring range, and the measurement values that the OD7000 produces
What is the light spot size of the OD7000s sensor heads?
Description
Tutorial
(Show all)How to insert and remove an OD7000 fibre correctly
Tutorial to guide the user through the correct procedure to insert and remove the sensor head fiber of an OD7000 controller
How to obtain a single measured value with OD7000
Description