distance sensors
Application
(Show all)Cooling plate and front heat protection (NIR filter) for the Dx50, DT50-2 and DT80
Details on cooling plates and NIR heat protection filters, including product variants and application-specific usage guidance.
Troubleshooting for SOPAS and IO-Link devices
Description
SIG200 Logic-Editor: SLT (smart-light-tower) indication for different distance values
Description
FAQ
(Show all)Is the LPC-DX50 and Control Panel Cover compatible with the Dx50-2?
Description
Is it possible to combine a laser triangulation based displacement sensor with a mirror?
Description
What is the diameter of the light spot for Dx50 / Dx50-2?
Description
Tutorial
(Show all)How to use Shape Mode of the DT50-2
Description