distance sensors
FAQ
Description
What is the maximum adjustment angle of the BEF-AH-DX50?
SOPAS provides a login function for devices. The Dx35 and Dx50-2 have no login level and therefore the function has no effect. All settings are available w
Description
Description
Description
Description
What is the input level for the MF input (active or inactive)
Description
Description
Where exactly is the optical axis of the Dx35 located?
Description
Description
Description
Description
Description