distance sensors
Application
(Show all)This article describes a special feature with regard to the 25-bit GRAY data format for the DME3000, DME4000 and DME5000 distance sensors.
This article describes how distance sensors from the DME4000/DME5000 device series with HIPERFACE® interface can be replaced by the successor DL100 Pro.
This article describes the restart behavior of DME4000/DME5000 distance sensors after the internal temperature dropped below -15°C.