Your SICK ID gives you access to our extensive range of services. This includes direct online orders, price and availability checks, and access to our digital services.
Merge of parameter "FieldEvaluationApplicationState" with "DeviceNotReady"
Article No: KA-09529
Version: 1.0
Subject to change without notice
Related Products
multiScan100
Table of Contents
In the firmware versions 2.0.0/ 2.0.1 of the multiScan, the Object Detection included the FieldEvaluationApplicationState, which indicated the availability of the field evaluation. In addition to the DeviceNotReady, this state could also be selected as a source for the digital outputs. Since V2.1.0, the FieldEvaluationApplicationState is linked to the DeviceNotReady signal and is no longer available as source to minamize the complexity of the multiScan error handling.
However, if the FieldEvaluationApplicationState was selected as a I/O-source signal in V2.0.0/ 2.0.1, the FieldEvaluationApplicationState remains as the IO source, even though it is no longer set by the device.
To fix this issue a reset to factory default is necessary.
Keywords: field evaluation, 3d object detection, Source, Input, Output