Your SICK ID gives you access to our extensive range of services. This includes direct online orders, price and availability checks, and access to our digital services.
This page helps you retrofit a TiM3xx / TiM7xx application where field evaluation is used.
Related Products
picoScan100
Table of Contents
General Information
All picoScan150 performances level (Core, Prime, Pro) can be used to retro fit a TiM3xx / TiM7xx. However, make sure the variant you use has the object detection / field evaluation feature onboard.
The TiM3xx/7xx uses 16 so-called field sets. A field set consists of three evaluation fields. You can only activate one of these field sets at a time by connecting the four inputs (2^4 = 16 field sets). Each field in each field set is permanently connected to a digital output (field 1 = output 1, field 2 = output 2, field 3 = output 3).
The picoScan150 uses groups instead of field sets. However, a group is still a collection of evaluation fields that can be activated by a trigger (e.g. freely configurable input combination, telegram, always active, ..). Several groups can be active at the same time. A group can have several (more than 3 possible) evaluation fields. Evaluation fields are no longer permanently connected to outputs. Several evaluation fields can trigger a specific output.
The attached .sopas file (top right corner on this page) can be imported to a picoScan150 with SOPAS ET to retrofit a TiM3xx / TiM7xx.
Parameter
The following table shows the different parameters which are adapted in the .sopas file you can download at the top of the page.
Parameter (different from default)
picoScan150
TiM3xx / TiM7xx
Firmware
>=1.4.1
>= 5.1
Scan configuration
15 Hz / 0.33°
15 Hz / 1 °
15 Hz / 0.33°
15 Hz / 1 °
Echo filter
First Echo
not available
Contamination indication
Warning and Error disabled
not available
Scan range filter
-135° ... +135° (Field of view: 270°)
-45° ... 225° (Field of view: 270°)
Distance filter
0.05m ... 25.00m
always 0.05m ... 25.00m
Output format
LMDscandata
always LMDscandata
Connector pinning (picoScan150 vs. TiM3xx/7xx)
Make sure you use the right system plug (PN: 2130871) which provides the best compatibility for TiMs. The following information on the left side always refer to the picoScan150 while the information on the right refer to the TiM3xx / TiM7xx.
Also note: While the TiM3xx/7xx had designated inputs and outputs (4 Inputs, 4 Outputs) the picoScan150 has only 6 Ports (Input or Output) due to hardware limitations. Therefore the provided .sopas file uses the following I/O assignments:
- Pin ③ = In1
- Pin ④ = In2
- Pin ⑤ OUT1
- Pin ⑥ OUT2
- Pin ⑦ OUT3
- Pin ⑧ OUT4.
This also means that In3 and In4 do not exist and therefore the same input logic as with a TiM is not possible.
picoScan150
TiM3xx/7xx
PIN assignments Power I/O connection
① GND
② Vs
③ I/O 1
④ I/O 2
⑤ I/O 3
⑥ I/O 4
⑦ I/O 5
⑧ I/O 6
⑨ n.c.
⑩ n.c.
⑪ n.c.
⑫ n.c.
Connecting cable with male connector or M12 male connector, 12-pin, A-coded
① GND
② DC 9 V ... 28 V
③ In1
④ In2
⑤ OUT1
⑥ OUT2
⑦ OUT3
⑧ OUT4
⑨ PNP: INGND, NPN: IN 9 V ... 28 V
⑩ In3
⑪ In4
⑫ n.c.
Connecting cable with male connector or M12 male connector, 12-pin, A-coded
Inputs settings
picoScan150
Both inputs (out of six I/Os) activate 2^2 = four groups, each with three evaluation cases/fields. The assignments are made in group settings. An example is shown below. If more input combinations are needed, the Ports (I/O) need to be assigned to an input first (Configurations --> Inputs and outputs).
TiM3xx/7xx
Output settings
picoScan150
TiM3xx/7xx
Field geometries
picoScan150
The picoScan150 use groups to combine several fields (TiM fieldsets).