OLS - BarCode
Related Products
Table of Contents
Today, I want to provide some information about the barcode our OLS can read.
I have done that in form of a "FAQ" list, if something is missing, please let me know.
- Which kind of BarCode is used?
- Which Orientation?
- Reading tolerance?
- How many digits can the OLS read?
- How to decrypt the 2/5 interleaved BarCode:
- Code with CheckSum
Which kind of BarCode is used?
interleaved 2 of 5
The code is called 2/5 interleaved, because there are 2 numbers coded by use of 5 bars.
1st Number = 5 x black bar
2nd Number = 5 x space in-between
With that method a high code density can be reached.
Which Orientation?
The barcode should be upright to the guiding line - so that the light spot of OLS goes through directly.
It doesn't matter if the code is turned 180° - our OLS is automatically recognizing the orientation and sets a flag "code flipped" in case of 180° turn
Reading Tolerance?
As written in the datasheet: 100mm +/-10
I want to advice that the code reading is less tolerant compared to the line guidance, that means that for >120mm there is no more reliable reading possible.
How many digits can the OLS read?
Our OLS can read a 4 digit code in a range from 0 to 255 due to the limitation of 8 Bit.
The Code is included in the process data.
For instance, in the CANOpen TPDO 1 - look for Byte 7 & Byte 8
How to decrypt the 2/5 interleaved BarCode:
Look here to see the construction of the code:
Start: bar - gap- bar - gap - all narrow
Stop: wide bar - narrow gap - narrow bar
The numbers are coded as follows:
n = narrow
w = wide
Our example with "1234" is just for demonstration - I want to mention, that 1234 is a too big number for the OLS (maximum = 255)
Code with CheckSum
To get the code reading more reliable, the 2/5 interleaved Code can be extended with a CheckSum
Here you can see an example how the CheckSum works:
All odd numbers are multiplied by 3.
The CheckSum Code is different to the normal Code and the OLS must be able to read such a Code with CheckSum.
Please be aware, that our standard OLS don't support CheckSum Codes.
But we can offer another OLS20 type on request, when needed.
ols, barcode, reading tolerance, code, checksum, decrypt