Your SICK ID gives you access to our extensive range of services. This includes direct online orders, price and availability checks, and access to our digital services.
There is a large IODD selection for the Dx35. Two points must be taken into account in order to transfer the appropriate IODD to the system:
Choose whether to use IO-Link V1.0 or IO-Link V1.1 - there is an IODD for each variant. Please note that sensors before SN 2034xxxx only support IO-Link V1.0!
Selection which DeviceID is to be used! A DS35 or a Dx35 Extended device can be created from a DT35 with the corresponding IODD (via DBC). When selecting the IODD, it is important to pay attention to the DeviceID (not just the name). See in the table below the corresponding sensors with their Device ID:
Device
DeviceID
Function
DS35 / DR35
6488070 (630006h)
IO-Link output
DT35 / DL35
6488065 (630001h)
IO-Link and analog output
DX35-Extended
6488071 (630007h)
IO-Link and analog output + additional process data