What is the cause of the SOPAS ET error message "No matching device type" when importing a Dx1000 project file?
This article describes the reason for SOPAS ET error message "No matching device type" and shows a possible workaround.
Related Products
Dx1000
Table of Contents
With SOPAS ET, among other things, parameter sets of devices can be exported and transferred (imported) to devices of the same type. It may happen that SOPAS ET rejects the import despite identical devices and instead displays the error message "No matching device type". This can be caused by different firmware versions of the export device and the import device.
Example for export device FW V1.5.0 and import device FW V1.10.0:
Example for export device FW V1.5.0 and import device FW V1.10.0:
- Export / Import of project in file format *.sopas:
Different file formats can be selected for export to the storage medium. SOPAS ET suggests the format SOPAS (*.sopas) by default.
Import of project on device with newer FW V1.10.0:
The import is aborted with the following error message:
- Export / Import of project in file format *.sdv:
Import project file on device with newer FW V1.10.0:
The import was carried out successfully.
Keywords:
export, import, no matching device type, sopas, project
export, import, no matching device type, sopas, project