web
You’re offline. This is a read only version of the page.
close
Support Portal

Milestone Plugin

Related Products
TiM
LMS1xx
LMS5xx
MRS1000

Table of Contents

Milestone Plugin

Software of 3rd Party which Supports our laserscanners for a Videomanagement Tool of Milestone. 

Milestone certificate:

 Please check the attachment


Version 3.6 R01

Software: 

Operating Manual:

Hint to add "SICK processing server":

 

The processing server is registered with the Milestone Download Manager when the plug-in is installed.

The installer can then be downloaded from the website http://milestoneServer/Installation and can be executed

In any case, it is recommended to do this for several scanners, otherwise the CPU load might be too high.

The configuration is then described in the BA from page 20 onwards. You can simply go and move the scanners to the new Processing Server

ATTENTION - The address for the camera stream must then also be adjusted IP/Port.

 

 

Older Versions can be requested over the SICK Support!

Keywords:
Camera systems, Video, Plugin