Your SICK ID gives you access to our extensive range of services. This includes direct online orders, price and availability checks, and access to our digital services.
[IPCam] Renaming not successful with Axis IPCam and SIM2000-p
Article No: KA-09427
Version: 4.1
Subject to change without notice
SIM2000-p was not able to rename the image stored by the IPCam
Related Products
VMS4130-BAA0, NON-LFT KIT, SIM2000-P QD
Table of Contents
SIM2000-p was not able to rename the image stored by the IPCam
The IPCam is sending images to the FTP Server but the file name is not correct.
Indicator for this issue:
Successful Image Request from IPCam is counting up
Save image failed is not counting up!
Renaming was not successful counting up
Names of the filename is not correct. Is the file name the default filename? [SIMNAME]_[DATE]_[TIME]_[ON].jpg or something different?
1. Validate if the credatials of the SIM are correct
2. Validate if an firewall is active. If yes check if the rename transfer is working without the firewall. If this is the case, set up the specific firewall rules
3. Please validate if the images are in the same folder as the rename command goes to