web
You’re offline. This is a read only version of the page.
close
Support Portal

mounting suggestion for motor feedback systems, encoders

How a motor flange (on encoder side) has to be designed, that a motor feedback system (encoder) can be mounted
Related Products
motor feedback systems

Table of Contents

The universal mounting suggestion, to fit most of the rotative encoders

The drawing is also available in the attachment.

If the motor flange is designed like this, it is possible to mount following motor feedback systems:

  • SEK37 / SEL37
  • EES37 / EEM37
  • SKS36 / SKM36
  • EKS36 / EKM36
  • SRS50 / SRM50 (metal stator coupling, resolver stator coupling)
  • EFS50 / EFM50
  • EDS35 / EDM35
  • ENS35 / ENM35

Individual mounting suggestion SEL37 / SEK37 / EES37 / EEM37

What is important?

  • tolerance of the taper (-3 angular sec)
  • distance between the mounting surface and the middle of the taper (where the taper has a diameter of 6.5 mm)
  • the centering of 33 mm, to keep the encoder's housing in place

Individual mounting suggestion SKS36 / SKM36 / EKS36 / EKM 36

What is important?

For the mounting of the EKx36 and SKx36 are only the inner mounting holes required (red circle). The hole circle is "38mm". The outer holes are for the mounting of the SRx50.

  • tolerance of the taper (-3 angular sec)
  • distance between the mounting surface and the middle of the taper (where the taper has a diameter of 6.5 mm)
  • position of the mounting holes

Individual mounting suggestion EDS35 / EDM35

What is important?

  • tolerance of the taper (-3 angular sec)
  • distance between the mounting surface and the middle of the taper (where the taper has a diameter of 6.5 mm)
  • position of the mounting holes

Individual mounting suggestion SRS50 / SRM50 / EFS50 / EFM50

with spring mounting plate

with resolver support

What is important?

  • The red marked distance can be higher. This is not a must requirement.
  • tolerance of the taper (-3 angular sec)
  • distance between the mounting surface and the middle of the taper (where the taper has a diameter of 6.5 mm)
  • position of the mounting holes

Individual mounting suggestion SES70 / SEM70 / SES90 / SEM90

SES70 / SEM70

SES90 / SEM90

What is important?

  • the diameter of the shaft (tolerance h6)
  • the shape and the depth of the centering, that the mounting is working
  • the position of the mounting holes
Keywords:
sks36, skm36, eks36, ekm36, sek, sel, ses, sem, ees37, eem37, srs50, srm50, eds35, edm35, ens35, enm35, mounting, motor feedback systems, motion and drives, hiperface, hiperface dsl