web
You’re offline. This is a read only version of the page.
close
Support Portal

Tutorial SIG300 (4/5) – Setting up an MQTT Client

This video covers: Connecting the SICK MPB10 vibration sensor to the SIG300. Configuring the SIG300 using the IODD file for the connected device. Setting up IO-Link ports and enabling necessary access rights. Configuring the MQTT Broker and connecting the SIG300 as an MQTT Client. Publishing sensor data to MQTT topics and visualizing it using MQTT Explorer.
Related Products
MPB10-VS00VSIQ00 MULTIPHYSICSBOX
SIG300

Table of Contents

In this video, you'll learn how to set up an MQTT Client on the SIG300 for efficient data communication.

 

The SIG300 is a versatile 8-port IO-Link Master. It seamlessly integrates sensors and actuators into fieldbus and IT systems.

 

This tutorial is perfect for anyone looking to integrate MQTT communication with the SIG300.

 

This video covers:

 

 

  • Connecting the SICK MPB10 vibration sensor to the SIG300.
  • Configuring the SIG300 using the IODD file for the connected device.
  • Setting up IO-Link ports and enabling necessary access rights.
  • Configuring the MQTT Broker and connecting the SIG300 as an MQTT Client.
  • Publishing sensor data to MQTT topics and visualizing it using MQTT Explorer.

 

By the end of this tutorial, you'll be able to use the SIG300 to send IO-Link process data via MQTT and visualize this data using MQTT Explorer.

Keywords:
SIG300, integration products, network and connection technology, network devices, io-link master, io-link, data processing, sensor integration gateway, data integration, industrial automation