web
You’re offline. This is a read only version of the page.
close
Support Portal

Is there an overview for the minimum drive shaft length for all through hollow shaft encoders?

Table of Contents

Please note:

The greater the installation depth or the more the drive shaft is located in the hollow shaft of the encoder, the better the performance of the encoder and the fewer electrical and mechanical problems will occur.

 

For this reason please always make for encoders with a through hollow shaft sure that the drive shaft is as long as possible.

As a recommendation, the drive shaft should be at least as long as the through hollow shaft of the encoder.

Encoder

Minimum Drive Shaft Length*

[mm]

DFS60S Pro

AFx60S Pro

SFx60

DFS60

AFx60 SSI

DFS21

ARS60

15

DUS60

DBS60

15 (front clamping)

54 (back clamping)

DGS80

25

ANx58

20

DGS90

60

*         With standard stator coupling

 

List last updated in August 2025

Keywords:
rotary encoders, hollow shaft encoders, blind hollow shaft, through hollow shaft, overview, minimum drive shaft length, minimum installation depth, maximum drive shaft length, maximum installation depth