web
You’re offline. This is a read only version of the page.
close
Support Portal

Release notes CDF600 EtherCat

Release Notes CDF600-0300
Related Products
CDF600-0300 CONNECT. DEV. FIELDB.
CDF600 EtherCAT
Attachments
ApplicationNoteFWUpdateCDF600-03.pdf
CDF600-EtherCAT-keyfile.zip
FWP-V1.20-EtherCAT.zip
FWP-V1.30-EtherCAT.zip
Packageloader_V27.zip

Table of Contents

General information

To update a CDF EtherCAT you have to use Packageloader V2.7 (see attachments). The update is done via Serial Aux (M8 Port) at the CDF600-03. See attached Application Note on how to update the CDF600-0300. An update via SOPAS ET or higher version of the Packageload is not possible!
The date given at the table indicates the date of publication and not the date of introducing new software.

 

Software Versions

 

Firmware Version Release Date Firmware Package Keyfile Comments
V1.20 21.01.2016 FWP V1.20 CDF600_Key
  • Use address switches for device identification - EtherCAT Station Alias
V1.30 09.09.2019 FWP V1.30 CDF600_Key
  • Increase time out for save permanent feature
  • Allow bus communication if sensor is lost in proxy mode
Keywords:
Key file, Release note, EtherCAT, Firmware, JAR, SDD, SOPAS, cdf600, CDF600 EtherCAT, cdf ethercat