web
You’re offline. This is a read only version of the page.
close
Support Portal

Is it possible, to cut the magnetic tape of a TTK70, TTK50, STL70, ETL70 into pieces and use the single pieces as measuring track?

Is it possible, to cut the magnetic tape of a TTK70, TTK50, STL70, ETL70 into pieces and use the single pieces as measuring track?
Related Products
TTK70
TTK50
STL/ETL70

Table of Contents

On the magnetic tape of the TTK50, TTK70, STL70, ETL70 is an magnetic absolute code.

It is possible to cut a longer tape into pieces, and use the single small pieces as measuring tracks.

On each piece is a different part of the code.

 

Info: It is not possible to make a measuring track out of several tapes (you will get position jumps and measuring errors at the connection between the 2 tapes) 

 

The minimum tape length looks like this:

--> meauring track + sensor length + 2*5mm

(see the picture)

Keywords:
magnetic tape, cut the magnetic tape, etl70, ttk70, measuring track, magnetic absolute code, ttk50, etl70, Hiperface, Hiperface DSL, Liner Encoder, motor feedback