web
You’re offline. This is a read only version of the page.
close
Support Portal

How to use RFH5xx with SOPAS ET

Short introduction how to use the RFH5xx with SOPAS ET
Related Products
RFH5xx

Table of Contents

SOPAS parameter description

The RFH5xx can be parameterized and used via SOPAS ET for demo puposes. The SOPAS parameters are described in the RFH5xx Parameter Description that can be found attached.

To use the RFH5xx with SOPAS ET the following acessory is necessary:

  • SiLink 2 USB-IO-Link Master + USB cable (SICK P/N: 1061790) 
  • RFH5xx device
  • standard 4/5 pin cable to connect RFH5xx to the SiLink Master

1) Connect the RFH5xx to the SiLink2 Master and connect the Master with your PC.

2) Open SOPAS ET.

If the RFH5xx is not found automatically via SOPAS ET, please do the following steps:

3) Open the "Search settings" in SOPAS in the lower right corner.

4) Select the option: "interface oriented search". 



5) Select IO-Link communication.


6) Finish the process and wait for the device to be found. 

Upload .sdd file

Make sure that the correct *.sdd file is integrated in SOPAS ET. The *.sdds for using the RFH5xx with SOPAS ET can be found in the download section on sick.com.

Save permanent

Please be aware, that the "save permanent" functionality is not necessary, because if a parameter is changed in IO-Link, this is always stored permanently, if not specified differently.

Userlevel & Passwords

Following userlevels and corresponding passwords are available in SOPAS ET: 

userlevel password
Maintenance maintenance
Service service

 

Keywords:
RFH, RFH5xx, RFH505, RFH510, RFH515, SOPAS ET, SiLink