web
You’re offline. This is a read only version of the page.
close
Support Portal

The article provides an approach to reset the analogue output of the Power Prox Sensor WTT12L.

The article provides an approach to reset the analogue output of the Power Prox Sensor WTT12L.
Related Products
WTT12L-B2546 PHOTOE.PROX.SWITCH
WTT12L-A2533 PHOTOE.PROX.SWITCH
WTT12L-A2543 PHOTOE.PROX.SWITCH
WTT12L-A2563 PHOTOE.PROX.SWITCH
WTT12L-A2553 PHOTOE.PROX.SWITCH
WTT12L-A2513 PHOTOE.PROX.SWITCH
WTT12L-A3543 PHOTOE.PROX.SWITCH
WTT12L-A1563 PHOTOE.PROX.SWITCH

Table of Contents

How to reset the analogue output of the Power Prox Sensor WTT12L.

 


 To reset the analog output: If the target is not moved during the teach process (or if it is moved less then 50 mm), then the minimum sensing range is assigned to 0V/4mA, the maximum sensing range is assigned to 10V/20mA (like factory setting).

 

Keywords:
Powerprox sensor, analogue version, factory reset , analogue output, power prox sensor, reset the analue output