Support Portal

Inspector83x firmware releases

Firmware for Inspector83x.
Related Products
Inspector83x

Table of Contents

Firmware file and installation

The Inspector83x firmware file is linked to through the Download button at the bottom of this article. The zip file consists of firmware file (.spk), API documentation and release notes.

Installation

Use the SICK AppManager software to update the firmware in a device.
In the SICK AppManager, do the following to update the firmware:

  1. Connect to the device.
  2. Clear apps and user data on the device before upgrading to ensure disk space availability (recommended)
  3. Import the firmware package (*.spk file) to the right pane named “Firmware” using the “Add Packages to repository”/+ button or drag-and-drop.
  4. Select the firmware package, then press “Install” to start the firmware update.

Inspector 83x firmware release V3.12.4

- Flicker-free illumination always on V2D8301

- Low Resolution Color variant

- Binning support for V2D8305 color devices

- New device specific cyber security configuration page

- AppEngine 3.16.0

- Bug fixes

Inspector 83x firmware release V3.11.1

- Support for on-device AI Object Detection and (AI Object Detection (dStudio) is already supported with 3.8.2) in Nova 2.10.

Inspector 83x firmware release V3.8.2

- Fixed Edgematcher (Object locator) scaling causing wierd matches and low score.

- Fixed digital output stop working if illumination type changed without first deactivating the output.

- AI Object Detection (dStudio) in Nova 2.10 is supported in this version (please note that on-device AI Object Detection is not supported - please use 3.11.1 or later).

Inspector 83x firmware release V3.7.0

Keywords:
firmware, inspector83x, firmware release, inspector83x firmware, inspector83x firmware release