Your SICK ID gives you access to our extensive range of services. This includes direct online orders, price and availability checks, and access to our digital services.
SOPAS ET has the option of recording process data and other sensor parameters using the "Data recorder" tool. To do this, Sopas must be started and the corresponding sensor added to the current SOPAS project. Click on "Data recorder" in the bottom left corner of the SOPAS window to open the tool. The individual settings for recording the data can be made by clicking on the settings icon.
When making the settings, it is important to create a file into which the recorded data should be written. In my example I use the .xlsx format. In addition, "IOLinkProcessDataInputFT2V6" must be checked so that the process data is recorded.
After confirming the settings, recording can be started by clicking on the recording icon. The recording can be stopped by clicking on the Stop symbol.
The recorded process data is saved as individual bytes. To interpret these bytes, they can be copied into the attached Excel file.