Your SICK ID gives you access to our extensive range of services. This includes direct online orders, price and availability checks, and access to our digital services.
picoScan150 - Differences in software settings compared to TiMxxx
Article No: KA-08422
Version: 2.0
Subject to change without notice
This tutorial shows the differences between the picoScan150 Core software settings compared to a TiMxxx.
Related Products
picoScan100
Table of Contents
Introduction
This tutorial shows the differences between the picoScan150 Core software settings compared to a TiMxxx. In this case, we compare a picoScan150 Core (FW V1.0.2) and a TiM781 (FW 5.02). However, the information also applies to most other picoScan150 and TiM4/5/7 variants with the latest firmware. We'll go through different settings as in a real customer setting.
The goal is to:
Login as Service
use CoLa B
use 15Hz of scanning frequency and 0.33° of angular resolution
limit the device to a field of view of 185° forward facing
only use the first echo
set filter
output distance and RSSI data
output the data in LMDscandata format
Login
TiM781
picoScan150
The default passwords are identical.
Differences
While Service is available with default settings the other user levels need to be activated before they can be used.
CoLa B
TiM781
(Find the setting: Parameter --> Network / Interface / I/O)
-->
picoScan150
(Find the setting: Configuration --> Connection options --> legacy protocols)
Differences
For the TiMxxx, the default ports (2111 and 2112) are always set to Cola A. For the picoScan150 these are different (see the picture above) and can not be changed with FW V1.0.2.
Scanning frequency and angular resolution
TiM781
The TIM uses 15Hz of scanning frequency and 0.33 ° of angular resolution as a default setting. This is not changeable.
picoScan150
The picoScan150 uses 15Hz of scanning frequency and 0.33°/1° of angular resolution as a default setting. This is changeable.
(Find the setting: Parameter --> Data processing --> Output data range)
picoScan150
(Find the setting: Application--> Data output --> Angle range filter)
Differences
As the coordinate system changed, you need to set different values to reach the same result with the picoScan150. The LMDscandata output format of the picoScan still uses the TiMs convention (-48° to 228°).
For the picoScan150 the filter needs to be activated, this was not necessary with the TiMxxx.
The TiM781 does not have multi-echo technology. Hence, there is only one echo. To have the same behavior with the picoScan150 you need to activate the Echo filter and set it to either first or second echo. Otherwise, you get a lot more output data.
Filter settings
Filter
TiM781
picoScan150
Notes
Edge filter
yes
no
Median Filter
yes
no
on the road map
Moving average filter
yes
yes
-
Interval filter
yes
yes
-
Angle range filter
yes (named output data range)
yes
-
Particle filter
yes
yes
-
Fog Filter
no
yes
-
Echo Filter
no
yes
-
Cuboid area filter
no
yes
-
Distance filter
no
yes
-
LMDscandata output
TiM781
The TiM always outputs the distance data by default. The RSSI data, the device name and the timestamp can be activated if needed.
The TiM always outputs the data by default.
picoScan150
The default format is Compact. Therefore you need to set it to LMDscandata.
The picoScan150 outputs the RSSI data by default and can not be deactivated with FW V1.0.2. The picoScan150 does not output the device name and this timestamp
with FW V1.0.2. However, it outputs "Time since start-up in us" and "Time since transmission in us" at the corresponding position.
Differences
The default format is Compact. Therefore you need to set it to LMDscandata.
The picoScan150 has a larger field of view. Therefore, there are an additional 54 bytes (18 beams * (2 bytes per distance value + 1 byte RSSI value))
Due to the higher measurement range, distance values can reach up to 65m (65535 mm). With range extension mode the maximum distance is 120m and the scale factor in LMDscandata is set to 2 (maximum value in telegram: 65655)
The picoScan150 does not output the device name and the timestamp with FW V1.0.2. If you activate these options in the TiM the output telegram gets longer and therefore the byte difference between picoScan150 and TiM gets less than 54 bytes.