web
You’re offline. This is a read only version of the page.
close
Support Portal

[ICR8xx-4] Can not connect to ImageFTP

Find here possible informations to solve your issue regarding the image output to ImageFTP. There are 5 points you can check on your side.

Table of Contents

Connect an ICR8xx-4 to ImageFtp

If you can't connect your ICR to ImageFTP and receive the images, please check the following points:

 

1. Check if the IP-Adress of your PC / Notebook is in the range of the ICR

ICR 890-4

Your PC

 

2. Check if your network is set to private

Use Powershell to get your network information by using the command:

get-connectionprofile

If your network is on public use the below command to set it to private:

Set-NetConnectionProfile -Name "Nicht identifiziertes Netzwerk" -NetworkCategory Private

 

3. Check if the server-ip and port is the same in the ICR and ImageFTP

ImageFTP

ICR

You can may use port 2021 instead of port 21

 

4. Check if the user exists in the ImageFTP

User settings in ICR

User in ImageFTP

 

5. Check the Image Source and Image Assignment in the ICR

Ensure that the Image Source matches to the image below.

Ensure that the settings in the Image Assignment matches to the image below.

Important for commissioning

  • Set the image output always to "Every Trigger", do not use "Master Controlled"
  • Name Source should be always "Internal". Otherwise there can be an issue by creating the image-name.
 

Not successful with your investigations? Please create a ticket with following information

Keywords:
ICR, Troubleshooting, ICR8xx-4, ICR890-4, ICR890