web
You’re offline. This is a read only version of the page.
close
Support Portal

What resolutions are possible with the DGS80?

What resolutions are possible with the DGS80?
Related Products
incremental encoders
DGS80/90

Table of Contents

According to the typecode overview, the DGS80 is only available with 5 possible resolutions between 1024 and 8192 pulses per revolution.

But this is not the complete truth.

 

On request there are also other resolutions from 1 to up to 16384 pulses per revolution, divisible by 2, possible. 

If an odd resolution is needed, this has to be evaluated at first.

 

In this way, if a customer needs an odd resolution / a resolution that is not listed on the homepage, just let us know or contact the customization team directly.

Keywords:
DGS80, incremental encoder, encoder, resolution