web
You’re offline. This is a read only version of the page.
close
Support Portal

What´s the difference between DL100-xxxxx112 (PROFINET) and DL100-xxxxx212 (PROFINET-HF)?

Related Products
DL100-21AA2112 DISTANZ-SENSOR
DL100-21HA2112 DISTANZ-SENSOR
DL100-22AA2112 DISTANZ-SENSOR
DL100-22HA2112 DISTANZ-SENSOR
DL100-23AA2112 DISTANZ-SENSOR
DL100-23HA2112 DISTANZ-SENSOR
DL100-23AB2112 DISTANZ-SENSOR
DL100-21AA2212 DISTANZ-SENSOR
DL100-22AA2212 DISTANZ-SENSOR
DL100-23AA2212 DISTANZ-SENSOR
DL100-23HA2212 DISTANZ-SENSOR
DL100-23AB2212 DISTANZ-SENSOR

Table of Contents

DL100 Pro product portfolio contains two generally different PROFINET versions DL100-xxxxx112 (PROFINET) and DL100-xxxxx212 (PROFINET-High Feature). On first view both versions look the same. They offer the same range of  features and device parameters even if some of the parameter look slightly different in the corresponding device description GSD files. The significant difference is the PROFINET available Netload Class:
  • DL100-xxxxx112 (PROFINET): this initial version was introduced in year 2013 when there were no mandatory netload tests to get PI certification. This version has no PROFINET Netload Class specification.
  • DL100-xxxxx212 (PROFINET-High Feature): this version was introduced in year 2018. Due to improved hardware it´s conform to highest available PROFINET Netload Class 3 (Advanced robustness against netload). It offers a high safety margin for extended PROFINET use cases.

Please note: the two versions use different gsd files which are not compatible to each other.

 
Keywords:
dl100 pro, profinet, netload class, network load, netload robustness, gsd, gsdml, high feature, hf