web
You’re offline. This is a read only version of the page.
close
Support Portal

Steel industrie - Detection of steel slabs ( > 600°C)

Application to detect hot metallic objects used in the steel industry.
Related Products
WT45-P200S03 PHOTOE.PROX.SWITCH
WT45-R200S04 PHOTOE.PROX.SWITCH
WS/WE45-P260S01 PHOTOELECTRIC SWITCH
WS/WE45-S02 PHOTOELECTRIC SWITCH
BEF-KP-W45 COOLING PLATE

Table of Contents

In the steel industry, often the application is to detect very hot metallic objects.

 

So why is that application advanced:

 

1. The object is very hot, that means that the environment will be heated up. So the sensor must be cooled down by some accessories.

 

2. The target itself will have a strong radiation (especially in the infrared wavelength) So we cannot use an infrared sensor because he would fail switching on the object which sends infrared radiation. IR Filter in the sensor is necessary.

 

3. Due to the fact that the target and environment is very hot a glass lens is required.

 

Enclosed our recommendations of the devices which you can use and why you should use them.

 

1016031 WS/WE45-P260S01 / WS/WE45-S01 Special version with Red-light sender and receiver +IR-filter(scanning range ca. 35 m), usually the W45 Series are equipped with IR-Sender and Receiver to reach big scanning ranges<350m.

1015316 WT45-P200S03 DC10...60V PNP/Q & Q-output 

1015317  WT45-R200S04 UC24...240V Relais output
Both sensors mentioned before are for detecting of objects with very hot surfaces (> +800°C), visible red light, IR cut filter against heat radiation, glass cover lens 5mm thick, robust metal housing, dynamic front screen heating greatly reduces condensation during rapid temperature changes

2011435  BEF-KP-W45 liquid cooling plates for the sensor / housing                   

2019053 OBS-W45-H special protection dust protection tube with heat protected glass and Infrared blocking Filter

 

 

Keywords:
metal industrie, steel industry, detection of steel slabs, hot metallic objects