web
You’re offline. This is a read only version of the page.
close
Support Portal

How to switch on/ off the sender laser via IO-Link

Related Products
OD200

Table of Contents

Some applications require to switch on and of the emitting laser during operation.
There are two ways to implement this for the OD200:

  • Using the physical multifunctional input of the sensor
  • Sending a specific command via IO-Link

In case you wish to control the sensors laser via IO-Link you need to send a binary 0 (to switch on the laser) or a binary 1 (to switch off the laser) via the process data output to the sensor.

You can find more information in the IODD overview document of the corresponding sensor:

Keywords:
sender, laser, io-link