Can the capacitive sensor CM30 operate in an environment of 0.8 bar?
Can the capacitive sensor CM30 operate in an environment of 0.8 bar?
Related Products
BEF-EA-CM30 INSTALLATION ADAPTOR-CM30
CM30-16BNP-EWDS03 CAPACIT.PROXIM.SENSOR
CM
Table of Contents
The capacitive sensor CM30 should be able to work at 0,8bar without any change of performance.
If the pressure increase and create any issue, we would suggest to mount the sensor in sensor well or add protection cap on the front.
eg. Type: BEF-EA-CM30 #2043770
Keywords: