web
You’re offline. This is a read only version of the page.
close
Support Portal

Provision of an MJPEG live stream via HTTP or HTTPS

Related Products
SEC100-5C9D1SFZZZZ SENSINGCAM
SEC110-5C9D1SFZZZZ SENSINGCAM
sensingCam SEC100

Table of Contents

To enable viewing of the live stream via HTTP or HTTPS, the “MJPEG Stream (HTTP/HTTPS)” function must be activated in the streaming settings.

Accessing the live stream

Once activated, the live stream can be accessed using the following URL:

http://<IP-address>/liveView

or, if HTTPS is configured:

https://<IP-address>/liveView

Client capacity

A maximum of two clients can access the MJPEG stream simultaneously.

Keywords:
mjpeg, http, https, mjpeg stream