web
You’re offline. This is a read only version of the page.
close
Support Portal

Where can I find the right IODD for the Dx35?

Related Products
Dx35

Table of Contents

There is a large IODD selection for the Dx35. Two points must be taken into account in order to transfer the appropriate IODD to the system:

  1. Choose whether to use IO-Link V1.0 or IO-Link V1.1 - there is an IODD for each variant. 
    Please note that sensors before SN 2034xxxx only support IO-Link V1.0!

  2. Selection which DeviceID is to be used!
    A DS35 or a Dx35 Extended device can be created from a DT35 with the corresponding IODD (via DBC). When selecting the IODD, it is important to pay attention to the DeviceID (not just the name). See in the table below the corresponding sensors with their Device ID:

    Device
    DeviceID
    Function
    DS35 / DR35 6488070 (630006h) IO-Link output
    DT35 / DL35 6488065 (630001h) IO-Link and analog output
    DX35-Extended 6488071 (630007h)

    IO-Link and analog output
    + additional process data

 

The IODDs are available on the SICK website or via the IODDfinder.

Keywords:
iodd, dbc, deviceid