Support Portal

picoScan100: How-to videos?

This extensive collection of picoScan100 video tutorials is designed for users of all levels, from beginners to advanced. These language-neutral videos (without sound) will guide you through everything you need to know while using a picoScan100.
Related Products
picoScan100
Attachments
picoScan100_networkScan.py
ScanSegmentAPI_process_compact_matplotlib.py
sick_scan_xd_api_pico.py

Table of Contents

Getting started & Basic Settings

How to connect?

How to search for the device with SOPAS ET?

How to login?

How to enable user levels?

How to change the device IP address?

How to change the device name?

How to change the scanning frequency and angular resolution?

How to reboot the device?

How to perform a factory reset?

How to install and establish a first device connection with SOPAS ET? 

How to import and export the configuration with SOPAS ET? 

How to create a device configuration offline and import it to an online device?

 

Date and system time

How to setup a device time?

How to enable PTP for time synchronization?

 

Filter

How to suppress a glass pane with multi-echo?

 

Contamination indication

How to receive the contamination indication states via event-driven Cola (A/B)?

 

Data output

How to enable measurement data (Compact, UDP)?

How to enable measurement data (LMDscandata, CoLa A, TCP)?

How to read and understand the output telegram LMDscandata?

How to use Wireshark to dissect the Compact data format?

How to receive IMU data and dissect them with Wireshark?

 

Field evaluation

How to draw fields and detect objects?

How to configure a field for retro-reflectors only?

How to use a teached background for field evaluation?

How to use a contour as a reference?

How to use the object history feature?

How to visualize the bounding boxes of the detection history?

How to setup an output?

How to activate fields via HTTP?

How to read the field evaluation state via HTTP?

How to receive the field evaluation state via event-driven Cola (A/B)?

 

Scan view

How to visualize retro reflectors?

How to use the measurement tool?

Application Programming Interface (API)

How to use the REST API client (sick_scan_rest_client)?

How to manipulate existing field contours via the REST API?

How to use the OpenAPI file with the API platform Insomnia?

Install Insomnia: https://insomnia.rest/download

How to install and use the Insomnia REST plugin?

How to use ScanSegmentAPI (Python)?

How to use ScanSegmentAPI and analyze measurement data including matplotlib (Python)?

also see https://github.com/SICKAG/ScanSegmentAPI and attached file on this page "ScanSegmentAPI_process_compact_matplotlib.py"

How to use ScanSegmentAPICSharp (C#)?

How to use sick_scan_xd to receive and plot measurement data including matplotlib (Python)?

also see https://github.com/SICKAG/sick_scan_xd?tab=readme-ov-file#complete-usage-example-in-python and attached file on this page "sick_scan_xd_api_pico.py"

How to discover picoScan100 devices in the network (Python)?

find the script attached to this page "picoScan100_networkScan.py"

 

Robot Operating System (ROS)

How to install (binaries) and run the ROS driver (sick_scan_xd) on Linux?

How to install (binaries) and run the ROS 2 driver (sick_scan_xd) on Linux?

How to build run the ROS 2 driver (sick_scan_xd) on Linux?

How to use native ROS 2 (DDS) on Windows?

How to use native ROS 2 (DDS) on Linux?

 

Firmware update

How to perform a firmware update with SOPAS ET?

How to perform a firmware update via HTTP?

 

Measurement samples

Indoor measurement data example

Outdoor measurement data example

Device and measurement data reliability

 

Diagnostics

How to read the internal device temperature?

 

Data recording

How to use ROS 2 to record and playback measurement data in rosbag format (.db3)?

This example uses a multiScan100 for showcasing the recording. The same approach can be used with the picoScan100. Also see: https://github.com/SICKAG/sick_scan_xd

How to use ScanSegmentAPI to record measurement data in JSON format (.json)?

How to use SOPAS ET to record measurement data in Excel / CSV format (.csv)?

 
Keywords:
picoScan, picoScan100, picoScan120, picoScan150, tutorial, video, video, explanation, help, driver, SOPASair, SOPAS ET, filter, measurement data, update