web
You’re offline. This is a read only version of the page.
close
Support Portal

Is there a tool for loosening and tightening M12 plug connectors available?

Is there a tool for loosening and tightening M12 plug connectors available?
Related Products
TORQUE SCREWDRIVER M12 PLUG CONNECTORS
TOOL-TW06M12AF13 TIGHTEN.TORQUE WRENCH
linear encoders

Table of Contents

Sometimes it is hard to tighten or to loose M12 plug connectors and even more if there is not much space for that.

But a tight M12 plug connector is important to achieve the specified IP-rating.

For this case there are two tools available.

 

The TOOL-TW06M12AF13 (left picture) is for M12 plug connectors with a tightening torque of 0.6 Nm, the Torque screwdriver with attachment for M12 plug connector (right picture) has a tightening torque of 0.4 Nm

Keywords:
M12, plug connectors, M12 connectors, cables, tools, 0.4 Nm, 0.6 Nm