Your SICK ID gives you access to our extensive range of services. This includes direct online orders, price and availability checks, and access to our digital services.
Product comparison between LM31-450 and LL3-LM31450
Article No: KA-09853
Version: 1.0
Subject to change without notice
Related Products
WLL12-B5381 REF.PHOTOELEC.SWITCH
WLL12-B5271 REF.PHOTOELEC.SWITCH
LM31-450 FIBRE OPTIC CABLE
LM31-450M01 LICHTLEITER
LL3-LM31450 OPTICAL FIBER L=450MM
Table of Contents
The successor to LM31-450 is introduced as LL3-LM31450. Is it exactly the same in terms of performance, size, connection compatibility, etc.?
Answer:
It is the same fiber than the predecessor with only one difference. The connector is made for the new sensor amplifier familys like WLL180T, GLL170T, WLL80,.. and changed from
to
When using the old WLL12 amplifier, please use the old system ( LM31-450 phased out) or switch to the new system ( LL3 fibers with flying leads) with the adapter kit 2015210 AD-LL-2M2 that looks like this:
Fibers with a fix sensor input and no flying leads are not suitable for the adapter kits because the distance between sender and receiver on the sensor side is too small for the old WLL12.