web
You’re offline. This is a read only version of the page.
close
Support Portal

Outputs LMS53x

Related Products
LMS531

Table of Contents

Abstract

Description of the output function of the LMS53x.

 

Disqualification Output


That output has no special function in the LMS531. It is a standard output that can be used for all available functions (Field evaluation, Device Ready, Contamination, etc.). Just the standard defineds, that the outputs have  to have certain names. That are:

  • Alarm
  • Error
  • Sabotage
  • Disqualification

But that does not indicate a certain function.
The LMS1xx for example has no disqualification output, because that device has only 3 outputs (Alarm, Error, Sabotage), so a disqualification output was not possible.

Keywords:
Output, Disqualification output, Available functions