web
You’re offline. This is a read only version of the page.
close
Support Portal

What happens if you do a RESET at a wire draw encoder with analogue output?

What happens if you do a RESET at a wire draw encoder with analogue output?
Related Products
linear encoders
wire draw encoders

Table of Contents

If you have a BCG05-K1KM01PP (6039745) for example, then you have a device which is a combination of a MRA -G055-101D4 (5324019) and a ACM36-K1K0-K01 (6039751).

 

If you perform a RESET at a ACM36 which was sold without any wire draw mechanics, then the encoder is set to a measuring range of 16 turns. This means 4mA ... 20mA (0V ... 10V) within 16 turns.

 

If you perform a RESET at a ACM36 which is mounted at a BCG05, then the encoder is adjusted to the default settings of the wire draw mechanism-encoder combination.This is 0V/4mA at 0m and 10V/20mA at 1m.

Keywords:
reset, analogue output, wire draw encoder, HighLine, EcoLine, VarioLine