SRM50-FFA0-S01 (1034103) / SRM50-FFA0-S21 (1037157) / SRS50-FFA0-S01 (1034168) / SRS50-FFA0-S21 (1037156) special encoders
Related Products
Table of Contents
The ...
The device SRM50-FFA0-S01 (1034103) is the old Generation 1 device and was replaced by the SRM50-FFA0-S21 (1037157) The device SRS50-FFA0-S01 (1034168) is the old Generation 1 device and was replaced by the SRS50-FFA0-S21 (1037156) See also the attached data sheets |
srs50, srm50, hiperface, special, customized, encoder, motor feedback, mfb, motion and drives,