web
You’re offline. This is a read only version of the page.
close
Support Portal

PeopleCounter: Upper bound of region of interest

How to use the upper bound of region of interest parameter for People Counter
Related Products
MRS1104A-111011P01 PECO SET 01
MRS1000A

Table of Contents

In rare cases, you may need to mount the People Counter on a low ceiling. If the mount height is lower than 2.2 m or there are other objects mounted on the ceiling hanging below 2.2 m, there are scan points in the ROI which are evaluated after every scan. This can cause reduced performance of the People Counter.

With the parameter "Upper bound of region of interest" you have the possibility to blank out this ceiling or objects. All scan points above the top blue line (the upper bound of region of interest) are ignored for the evaluation.

Keywords:
peoplecounter, people counter, mrs1000a, PeCo