Your SICK ID gives you access to our extensive range of services. This includes direct online orders, price and availability checks, and access to our digital services.
FastID is a feature supported by selected Impinj transponders, which allows the RFU6xx device to quickly access the transponders unique TID during an inventory operation. Normally the reading of the TID requires additional reading commands. If the FastID is activated the transponder answers with a combined EPC+TID information.
Benefits of FastID
improved reading speed - reading out the TID does not require an additional read TID command
Read transponders with same EPC - It is possible to read and distinguish transponders with the same EPC data since the TID information is unique for each transponder
How to activate FastID
FastID is available for firmware version V2.52 or newer for the following devices: RFU610, RFU620, RFU630, RFU650
This feature can be found on the SOPAS page "Transponder Processing" and can be activated as soon as a login as Service has been done.
The default password for the userlevel "Service" is "servicelevel".
After the activation of FastID the EPC contains also the TID of the transponder. For this example an Impinj M830 transponder was used.
Quickstart with disabled FastID
Quickstart with enabled FastID
⚠ Please notice that the Transponder Access page within SOPAS ET is not supporting FastID. Therefore accessing the tag via Tag Access will fail. However writing the EPC is still possible by commands or Tag-Processing.
Supported transponders
IC type
FastID supported?
FastID answer format
Comment
Monza R6
Yes
PC EPC TID
Monza 4E
No
Monza 4D
Yes with limitations
PC EPC CRC TID
Due to CRC, one word of TID is missing
Monza 4i
Yes with limitations
PC EPC CRC TID
Due to CRC, one word of TID is missing
Monza 4QT private Mode
Yes with limitations
PC EPC CRC TID
Due to CRC, one word of TID is missing
Monza 4QT public Mode
No
M730
Yes
PC EPC TID
M750
Yes
PC EPC TID
M780
Yes
PC EPC TID
M830
Yes
PC EPC TID
This is a not a complete list of transponders. If you have futher questions regarding compatibility please create a support ticket.