Your SICK ID gives you access to our extensive range of services. This includes direct online orders, price and availability checks, and access to our digital services.
that fits together in both directions of the protection hood. Mounting kit 3 does also fit here, but an upside down mounting of the sensor is then not possible becaus of the cables.
This is a mounting kit with the possibility for a fine adjustment of the sensor (roll angle +/- 3�, nick angle +/-2�)
This one fits directly on the sensor without any other bracket.
It works also in combination with the following other brackets in the shown order:
The standard mounting kit does not fit on the fine adjustment bracket.
The fine adjustment bracket can also be used in combination with the weather hood, but therefor the adapter bracket No. 2059271 is necessary:
Be careful how you mount the adapter 2059271. He is not symmetrical, so if you mounted it in the wrong way, the two attachments ("ears") for the connection box, will collide with the weather hood!