web
You’re offline. This is a read only version of the page.
close
Support Portal

SLG-2 StandAlone - how to configure Q2 to Pin 2 in SOPAS

This article explains how to configure Q2 to Pin" in SOPAS of a SLG2.
Related Products
SLG-2

Table of Contents

 

In some applications, Pin2 must be re-configured. Here I will show how to do that in SOPAS by example.
For the SLG2 the Pin2 configuration is implemented in a similar style as for the NextGen_AXX sensors.

Default setting

Status of all Qint

Can be seen under "Zones / Qints".
As you see, all Qints are configured for presence detection over the whole detection range.

 

Status Pin2

Under "Smart Task", Pin 2 is pre-configured as a Teach-in input.

 

How to connect QL2 to Pin 2

Go to "Smart Task".

In the default view you will see the following:

 

To configure the QL2 output to Pin2 we need 2 steps: 

Step 1: Click pull down "Selector 2" and select the needed Qint.

Step 2: click pull down "Pin2 configuration" and select "Switching signal QL2".

Result

Now Pin 2 is switching according to the Qint.2 setting = presence detection for the whole detection field!

 

Keywords:
sopas, ql2 to pin 2, configuration