picoScan150: No measurement data output
Related Products
Table of Contents
If the picoScan150 is not sending measurement data and the destination IP address is not visible in the Data Output tab under Measurement data output as in the following example:
There are several options for regaining the data output settings settings:
Methode A: Using provided programm
The simplest method is to use the picoScan150_Measurement_data_enable.exe file provided by your SICK support.
The correct setting option should then be visible again:
http://192.168.0.1/#/application/dataoutput
Methode B: REST/HTTP
For changing via HTTP/REST command please use the following command:
192.168.0.1/ ScanDataEthSettings
{
"data": {
"ScanDataEthSettings": {
"Protocol": 1,
"IPAddress": [
192,
168,
0,
100
],
"Port": 2115
}
}
}
More details see https://www.sick.com/de/en/downloads/media/swp678507 and https://support.sick.com/sick-knowledgebase/article/?code=KA-09302
Methode C: CoLa A/b
Method to update via TCP about CoLa binary (Port 2112) or CoLa ASCII (Port 2111)
CoLa ASCII example | |
Login | sMN SetAccessMode 04 81BE23AA |
02 73 4D 4E 20 53 65 74 41 63 63 65 73 73 4D 6F 64 65 20 30 33 20 46 34 37 32 34 37 34 34 03 | |
Set correct ethernet settings | sWN ScanDataEthSettings 1 C0 A8 0 64 843 |
02 73 57 4E 20 53 63 61 6E 44 61 74 61 45 74 68 53 65 74 74 69 6E 67 73 20 31 20 43 30 20 41 38 20 30 20 36 34 20 38 34 33 03 | |
Save permanently | sMN mEEwriteall |
02 73 57 4E 20 53 63 61 6E 44 61 74 61 45 74 68 53 65 74 74 69 6E 67 73 20 31 20 43 30 20 41 38 20 30 20 36 34 20 38 34 33 03 |
More details see chapter telegramlisting in the operating instruction and knowledge article https://support.sick.com/sick-knowledgebase/article/?code=KA-09481
Important!
If you reset the device to factory settings, you must repeat the procedure.
picoScan150, picoScan, LiDAR, measurementdata, UDP, troubleshooting,