web
You’re offline. This is a read only version of the page.
close
Support Portal

Passive Connectivity ==> bending radius, bending cycles, halogen-free, PUR, PVC

The article informs about passive connectivity and explains terms like bending radius, bending cycles, halogen-free, PUR & PVC.
Related Products
protective housing

Table of Contents

A system is only as robust as its weakest link. From this perspective, the quality and understanding of accessories such as connectivity become crucial. This gives us another reason to delve deeper into the realm of connectivity within this topic.

What does bend radius mean?

 In cable terminology, bend radius refers to the smallest curve that a cable may have when laid without changing the characteristics of the cable. Bend radii (Rmin) are specified in relation to the cable diameter (D) (see picture 1).

 

What does halogen-free mean?

Cables and wires are defined as halogen-free if they are made of materials that do not contain salt- forming chlorine, fluorine, bromine and iodine. The insulation and cladding of these cables are made of polymers based on pure hydrocarbons. When these materials burn, no corrosive or toxic gases, only water vapor and carbon dioxide are emitted.  The use of halogen-free cables becomes more and more compulsory with increasing numbers of buildings where people gather or everywhere, where safety consciousness to protect human life and valuable materials take a special significance. 

Halogen free cables are used in: 

  • Hospitals, airports, stores, hotels, theaters, schools, multistory buildings, fire warning plants, alarm systems, ventilation systems, escalators, elevators etc.

Humid Areas or maximum flexibility, use PUR cables!

Various industries e.g. Machinery- , plant- or tool making industries are working particularly with mineral oils, alkalis and aggressive coolant emulsions and under difficult environmental working conditions. Due to these conditions the electrical cables have to perform to exceptionally high standards. Flexibility, abrasion and oil resistance have to be guaranteed.

Material durability, PUR 

Flexible, silicone- and halogen-free cable with PUR outer sheath polypropylene conductor insulation. Oil and flame resistant in accordance with VDE 0472. Can be used in dragchain applications with minimal bend radius. This cable is very well suited for flexible applications in robotics, machine tools and metal- cutting manufacturing.

Material durability, PVC

Pure PVC cable, suitable for medium mechanical stress for packaging machine applications as well as assembly and production lines. Good resistance to acids and alkalis and therefore ideally suited for use in the food and beverage industry. Limited abrasion behavior and limited resistant to oil and chemicals.

 

IP enclosure rating:

IP enclosure ratings define the degree of protection (ingress protection) of the housing against contact, impurities and water. The first digit indicates the protection against mechanical impurities and the second digit indicates protection against water.

An important factor for reaching the indicated IP-enclosure rating plays the adherence to the proper tightening torque of the milled nut of the connection cable.

  • IP65: Protection against access with a wire, dust tight, protection against water jets (nozzle) from any angle. ?
  • IP67: Protection against access with a wire, dust tight, Protection against temporary immersion in water (depth of 1 m, 30min). ?
  • IP68: Protection against access with a wire, dust tight, Protection against continuous immersion in water (requirements must be higher than IP67). ?
  • IP69K: Protection against access with a wire, dust tight, Protection against water in high- pressure/steam cleaning applications (100 bar at 80�C) at various angles.

Important note:  Up to enclosure rating IP X6, all lower enclosure ratings are automatically covered. For higher enclosure ratings, this does not automatically apply to water protection ratings 7, 8 and 9K. If the inclusion of a lower enclosure rating is required, this must be specified with a dual designation.

Keywords:
passive connectivity, bending radius, bending cycles, halogen-free, PUR, PVC