web
You’re offline. This is a read only version of the page.
close
Support Portal

Tutorial SIG300 (4/5) – Setting up an MQTT Client

This video covers: Connecting the SICK MPB10 vibration sensor to the SIG300. Configuring the SIG300 using the IODD file for the connected device. Setting u
Related Products
MPB10-VS00VSIQ00 MULTIPHYSICSBOX
SIG300

Table of Contents

In this video, you'll learn how to set up an MQTT Client on the SIG300 for efficient data communication.

 

The SIG300 is a versatile 8-port IO-Link Master. It seamlessly integrates sensors and actuators into fieldbus and IT systems.

 

This tutorial is perfect for anyone looking to integrate MQTT communication with the SIG300.

 

This video covers:

 

 

  • Connecting the SICK MPB10 vibration sensor to the SIG300.
  • Configuring the SIG300 using the IODD file for the connected device.
  • Setting up IO-Link ports and enabling necessary access rights.
  • Configuring the MQTT Broker and connecting the SIG300 as an MQTT Client.
  • Publishing sensor data to MQTT topics and visualizing it using MQTT Explorer.

 

By the end of this tutorial, you'll be able to use the SIG300 to send IO-Link process data via MQTT and visualize this data using MQTT Explorer.

Keywords:
SIG300, integration products, network and connection technology, network devices, io-link master, io-link, data processing, sensor integration gateway, data integration, industrial automation