web
You’re offline. This is a read only version of the page.
close
Support Portal

What happens when the internal memory of the sensingCam SEC100 is full or the max. number of elements has been reached?

Related Products
SEC100-5C9D1SFZZZZ SENSINGCAM
SEC110-5C9D1SFZZZZ SENSINGCAM
sensingCam SEC100

Table of Contents

When the internal memory (6 GB) is full and further events or snapshots are triggered, the oldest files are automatically deleted.

If the file size of the snapshots or events is so small (low resolution, high compression...) that the maximum number of 1024 files in the archive is exceeded, the oldest files are also automatically deleted.

 

Alternatively, the FTP/SFTP function can also be used to send files directly to the corresponding server without using the internal memory.

 

Keywords:
memory, storage, filelimit