web
You’re offline. This is a read only version of the page.
close
Support Portal

Is it possible to change the electrical interface of the DUS60?

Is it possible to change the electrical interface of the DUS60?
Related Products
incremental encoders
DUS60
linear encoders

Table of Contents

The type code of the DUS60 has in total 15 digits. The digit number 14 or let's say the second to last digit tells you about the DIP switch configuration.

If you check the type code in the product information you can see that only for the models with the letters

  • A
  • B
  • C
  • D

the output voltage can be selected.

To select the desired output voltage you need to configure the DIP switch number 8 as you can see on the following picture.

  • By default this DIP switch is set to position OFF. Therefore the output voltage is 5 VDC → TTL.
  • If this DIP switch is set to position ON the output signal is equal to the input voltage → HTL
Keywords:
DUS60, output voltage, electrical interface, HTL, TTL, dip switch